Part Number: TXB0108
Tool/software:

The OE pin is only connected to the VCCA power supply pin ,
Is that okay?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0108
Tool/software:

During power up (when VCCA is above 0 V but below 1.2 V), the outputs might not work correctly; therefore, it is recommended to pull OE low during power up.
If you do not care about the state of the outputs during power up, then you can connect OE directly to VCCA.