SN74LVCH16244A: ESD protection with device installed

Part Number: SN74LVCH16244A

Tool/software:

Hello, the SN74LVCH16244A datasheet in Section 7.2 states that the component is protected to 2000V HBM for "all pins," however I have a question on if the VCC pins are protected when the component is installed on a board as follows: If the GND pins are connected to a very low impedance ground plane, and if the VCC pin receives a direct injection of 2kV HBM with the I/O pins mostly floating, can the part still handle this?