This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC1T45: SN74AXC1T45 can be used for clock @ 320Mhz when translating from 2.5V to 1.2V ?

Part Number: SN74AXC1T45


Tool/software:

Hi , i have clock being generated from my FPGA for the DUT. The FPGA generates a 2.5V (LVCMOS) @ 320MHz , i need to voltage translate it to 1.2V ( LVCMOS ) @ 320MHz for the DUT.
Can SN74AXC1T45 be suitable for this application ?

In the data sheet it says 500Mbps when translating from 1.8V to 3.3V.
So what is the rate when translating from 2.5V to 1.2V.

Is SN74AXC1T45 can't be used please suggest a alternative which supports my application.

Thanks.