Tool/software:
Hello,
how is the following information in the data sheet regarding the current consumption of the IC to be understood?

Supply current Icc=10µA (max), but additional max. 500µA with any other input at exactly Vcc-0.6V? Or also with a lower voltage than Vcc-0.6V?
Wich inputs are affected? Let's say I want to use the IC as RS-flip-flop with either PRE#=low and CLR#=high, or PRE#=high and CLR#=low.
Will the current consumption then always be 500µA?
Regards, Oliver.