Tool/software:
Hi team,
Could you please help to recommend a device without internal pull-up resistor?
Other requirements:
I noticed the TXB0102 in our portfolio can met the requirement, could you please help to double confirm whether there is no internal pullup resistor?
BRs,
Rannie
The 4 kΩ resistor works as a pull-down or pull-up resistor, depending on the state of the pin on the other side.
You want the TXU0102.
Thanks for your reply.
I'm curious why the 4kOhm is PL/PH resistor? My understanding is like below:
You have marked the one-shot, which is activated only for a short time for signal edges.
The buffer with the 4 kΩ series resistor is always active, on both sides. This is the output, but with a very low drive strength. The resistor allows an external device to override the voltage at the pin (this allows bidirectional signals).
Hi Rannie,
Clemens is correct here. The 4k series resistor is implemented here by design and is considered to be "weak" such that it allows for inputs at either A/B side to change direction.
TXU0x02 follows the requirements given so far as fixed direction translators for GPIO signals without internal pullup resistors.
Regards,
Jack