This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCT240: Design Question

Part Number: SN74HCT240

Tool/software:

Hello team - can you help with the question below? Thank you

I was wondering whether the circuit shown below using SN74HCT240 is generally bad design practice on a single package?

  1. Multiple inputs are being tied together
  2. Multiple outputs are being tied together
  3. One output loops back to multiple inputs

 

This circuit is being used as a differential 5V switch.