Part Number: SN74LV1T08
Tool/software:
1. Input transition rise or fall rate is determined to be 20ns/V in the datasheet. Is this applicable between VILmax(0.8V)~VIHmin(1.35V)? Device is used under the condition of Vcc=3.3V, Vin =1.8V
2. under the above condition, the voltage difference is 1.35-0.8=0.55, therefore is the rise/fall time calculated as 20ns*0.55V=11ns?
3.what kind of issue can be expected if the transition time is exceeded?
Regards