Part Number: CD4070B
Tool/software:
Team,
Customer is currently designing the position resolver system of MD by using CD4070B for logic design.
1. In the below circuitry, The U pin of the 4070 is set at 2.5V initially. and U- is set at 2.496V . At this condition, the input condition falls in the undefined region (VIL,max = 1.5V as defined in d/s). In this status, the output of 4070 is pulled high by 3.3V via 4.7K pull-up resistor as circuit shown.
2. And also, when U and U- pin of 4070 are set at 1V, the IC falls in spec defined as VIL,max <1.5V,max. The 4070 is pulled to LOW state.
We just would like to confirm if above items are correctly?


Regards
Brian