Tool/software:
I see from another thread theta_ja, theta_jb, and theta_jc(top) for SN74LVC2T45MDCTTEP is 184, 96.4, and 114.7 °C/W respectively.
What is the maximum allowable junction temperature for the device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I see from another thread theta_ja, theta_jb, and theta_jc(top) for SN74LVC2T45MDCTTEP is 184, 96.4, and 114.7 °C/W respectively.
What is the maximum allowable junction temperature for the device?
Hello Bill,
The max allowable junction temperature will be equal to the max storage temperature (150C).
See FAQ for additional information:
[FAQ] What is the maximum junction temperature (TJMAX) for a device?
Regards,
Josh