Part Number: SN74ACT8541
Other Parts Discussed in Thread: SN74ACT244,
Tool/software:
Hi,
My project is using SN74ACT244. But there is a question, the /OE1 only controls 4 channel, /OE2 controls another 4.
The original design is to use /OE1 and /OE2 to form a AND gate to control 8 channels.
The buffer can output a high or low level only when both /OE1 and /OE2 are low.
So is it approriate to choose SN74ACT8541 to replace SN74ACT244.
My request:
1. Vcc is supplied by 5V.
2. Inputs are TTL-compatible
3. IOH and IOL is above ±20mA
Thanks