FAQ: Logic and Voltage Translation > > Current FAQ
- [FAQ] What are the differences between Ground-Level Translators and Digital Isolators?
- [FAQ] Can I generate a negative PWM signal from a positive PWM signal?
- [FAQ] Is DC ground shifting possible when both supplies are connected together?
- [FAQ] What is the maximum trace length ground-level translators can drive?
- [FAQ] Can TXG be used as a simple level translator / buffer?
- [FAQ] What is the leakage between 2 grounds?
- [FAQ] Will TXG QFN packages support wettable flank?
- [FAQ] How far apart can the two systems be with TXG I2C devices?
- [FAQ] Can TXG support IEC-ESD for offboard connections