This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Can TXG support IEC-ESD for offboard connections



FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

TXG devices (both push-pull and open-drain) cannot support any level of IEC-ESD. However, IEC-ESD can still be achieved by using a protection device like the ESDS30x product family. 

The ESDS30x family can support ±30kV contact and air gap discharge. The only drawback is the DC breakdown voltage of 4.5V (min). There is a possibility these device will start to breakdown before reaching 5.5V which is the max recommended voltage condition.