Part Number: SN74AVC4T245
Tool/software:
Hi Teams,
We find there are step waveform on slaver side, but there is normal waveform on master side.
Please refer schematic and waveform as following, thanks.
before level shift :

after level shift:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74AVC4T245
Tool/software:
Hi Teams,
We find there are step waveform on slaver side, but there is normal waveform on master side.
Please refer schematic and waveform as following, thanks.
before level shift :

after level shift:

How long are the traces between the level shifter and the slave device? What is their characteristic impedance? What is the distance between the level shifter and the three source termination resistors?
Do the waveforms become better or worse if you use 22 Ω instead?
Hi Clemens,
Reply as following, thanks.
1. How long are the traces between the level shifter and the slave device?
Total about 4800mils.
2. What is their characteristic impedance?
50ohm
3. What is the distance between the level shifter and the three source termination resistors?
Level shifter to master side termination resistor is about 1100mils , to slaver side termination resistor is about 150mils.
4. Do the waveforms become better or worse if you use 22 Ω instead?
Yes , I have tried to change 10ohm resistor to 22/50/100ohm, waveform changed better. Till to 100ohm , there is no this step noise.
Hello Che,
How fast are you running the device? The maximum trace length logic devices is 2350mils, see FAQ below.
[FAQ] What is the maximum trace length that a logic device can drive?
Regards,
Josh
Hello Che,
Sounds good. Let us know if there are additional questions we can help with.
Regards,
Josh