Tool/software:
Hello Team,
I am using the OR gate IC - CD54HC4075 in my design. Required cases for the IO logic are at 3.3V VCC which ain't mentioned in datasheet, please confirm if below numbers are ok to consider for design
Can you confirm if the below when operating at 3.3V VCC is as below;
-
VIH(min) ≈ 2.31 V (≈ 0.7 × VCC)
-
VIL(max) ≈ 0.99 V (≈ 0.3 × VCC)
-
VOH(Min)
≥ 3.13 V at IOH = –20 µA
≥ 2.9 V at IOH = –4 mA -
VOL(Max):
≤ 0.1 V at IOL = +20 µA
≤ 0.33 V at IOL = +4 mA
Confirm the above if correct, if not please provide at 3.3V
Regards,
Garima R.