This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E: TXS0108E

Part Number: TXS0108E
Other Parts Discussed in Thread: TXV0106

Tool/software:

Hello

I'de like to use TXS0108E  to interface from one side this FTDI chip  FT232H 3.3V and on the other side an 1.8V bank IO FPGA.

I'll use asynchronous FIFO protocol running around 12.5MHz

Regarding the TXS0108E datasheet timing characteristics it should be ok (from 1.8V to 3.3V it supports up to 60-70Mbps)  

As I will need to deal with 12 bits involved in async fifo protocol i ll need to use 2 TXS0108E  parts.

My question is : What is the part to part skew in the 1.8V to 3.3V translation (the DS only give the channel to channel skew : 1ns)?

Best regards