TXB0104-Q1: The risk and requirement for TXB0104QRUTRQ1 in TDM application

Part Number: TXB0104-Q1
Other Parts Discussed in Thread: TAS6424E, , SN74LVC1G08, TXB0104, SN74AXC4T245

Tool/software:

Hi team

My customer will use TXB0104QRUTRQ1 in below case which is shown in block diagram. 

The requirements of TAS6424E and TAS6422E are listed

1.TAS642x has MCLK and SCLK input pins but they can be connected together.

2.MCLK Trise/fall(10%-90%)  must be less than 5ns.

3.The maximum input currents are 15uA for TAS6424E’s MCLK/SCLK/Fsync/data

4.  

Would help confirm if TXB0104QRUTRQ1 is ok ? If it is ok, what's the requirements on TXB0104QRUTRQ1 and layouts?

Thanks