For the automotive-grade level conversion LSF0204-Q1, I would like to confirm whether the calculation of this PULLUP RESISTER is related to the On-state resistance
If the V_pass voltage drop is 0.35V, usually the Volmax of the MCU or SOC is around 0.3V. Thus, 0.35V+0.3V=0.65V, which exceeds the Vilmax of the MCU/SOC (for a 1.2V system, 0.3V is considered 0.36V). As a result, the level cannot be converted
Please provide a solution or recommend other suitable materials