Other Parts Discussed in Thread: TXB0108
Hi, I have a circuit where I run JTAG through the 74CBT to a TXB0108 part to translate the 3.3v to 2.5v to interface to a FPGA. Once the signal transistions to 2.5 volt it goes to a xilinx fpga.
I am running the JTAG as low as 750 Khz and still have the severe ringing - so it seems to be a voltage conflict between the devices, not a signal integrity issue per se.
Distance between the 2 parts is ~ 0.4 inch. We tried a series resistor of 50 ohm between the JTAG pod and the 74CBT device with no impact to signal ringing.
Basically the circuit is unuseable right now, I am in the midst of respinning the PCB and need to solve this issue. I don;t have board access between any of the parts as both are BGA devices, also there are no pullups or pulldowns on the signal lines, nor are there series resistors.
Thanks for the assistance.
Luke