This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUC1G08: skew

Part Number: SN74AUC1G08

I am looking for the package to package skew information for this part.  In my case the parts will be at the same temperature and supply settings.  Planning on 2.5V.   Really just need a buffer and the AND is the closest thing I could find.   Need the prop delay as I am passing 200MHz so the other families are too slow.   

In case there is a better solution: really need to go from LVDS to 2 single ended signals 1:2  and 2 in parallel so 2x 1:2 LVDS / LVTTL [or similar] would be ideal.  Barring that I am using a '28 to receive the two LVDS differential pairs and converting to single ended then the AND gates to buffer and keep from having stubs with the two end points for each.  Leading to my skew question.