Hi, I am unsure how the ioff partial power down mode works. Is it automatic upon removal of the power supply, the ioff circuit protects the device from voltages on the output lines. Does Vcc need to be at ground, or can it be floating. Also can the inputs be floating in the power down state. In essence if i disconect the cable which supplies the signals to the buffer, including the supply, will it enter the power down mode, and be safe against voltages on the output side of the buffer.
Regards, Jonathan