Other Parts Discussed in Thread: TXB0106
SCH.docxHi Team
My Question are write in Word file , Please help check
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
kerr - My feedback is below:
When initial, does the B side(net: SPI_SCK) is low to cause the 4K to GND? (and this is why we measured around 0.5V voltage which is divided 1.8v by 10K PU and 4K PD.)
Yes. Each TXB0106 I/O has a 4k series resistor. If a TXB input is driven low, then its output resembles a 4k pulldown resistor to GND. That could act as a voltage divider and keep the line low. The 'Detailed Design Procedure' of the datasheet specifies that pullups or pulldowns, if needed, must be greater than 50k.
kerr chang said:When does the one shot block active? And when one shot block active, it will cause the A side voltage keep on VCCA(1.8V)?
You can read this app note to under the one-shot architecture.
Best Regards,
Nirav
Hi Nirav
Looks like the A site pull high resistor will impact A site output VOH and VOL, as my understanding, according to our application, is that means the A site pull high resistor 3.3K ohm is ok if A site APU_SPI_SCK is always input?
Kerr,
In theory it should work. If the TXB0106 I/O is used exclusively as an input, then an external pullup resistor is acceptable as long as the SPI master can drive the TXB0106 I/O to valid VIH and VIL levels. I would like to verify this in the lab with a spot check just to make sure. I hope to get you results within 24 hours.
Best Regards,
Nirav