I\m looking for a solution to take 12 bit of data that come out of an MCU on rising edge and falling edge of the clock and do forward them into another IC that accepts only single clock edge data .... MUC is limited in Frequency <= 50MHz so SW change is not possible ... output of the device would need to double the clock then to 100MHz (40MHz to 80MHz might be as well sufficient).
Thanks a lot!