Part Number: CD4046B
Hi, I got the input from customer about VCO calculate even I check to application guide. But still confused about it. Can you help double check on it?
Thanks
Application - 4046 Phase Locked Loop as an FM Demodulator (Using phase comparator I for VCO with OFFSET)
To distinguish the input range in 400KHz,
Case 1: If input(pin14) range locate in Ftyp to Fmax, the P1(pin2) =1,
Case 2: If input (pin 14) range locate in Ftyp to Fmin, the P1(pin2)=0
Q1: How to calculate the value of R1,R2 and C1 to get the correct frequency as below?
Fmin=310KHz
Ftyp=383.8KHz
Fmax=471.194KHz
There have another tool we calculated as below. Is it correct?
Q2: If we do not need external low pass filter, can we keep floating? Currently, we connect R3,C2 as below.
R3 =18K,C2=220P ,fc=40.1KHz
Application - 4046 Phase Locked Loop for clock generator(Using phase comparator I for VCO with OFFSET)
Use CD4046B pin2 to generate the frequency about 300KHz, MCU GPIO will send the signal to CD4046B pin5 (Inhibit) and pin14 keep external pull high.
In case pin5 (Inhibit) receive =1 high from MCU, P1 should output the frequency.
Q3 : In this case, can we floating the Pin2 and pin9 if do not connect to low pass filter?
R1,R2,C1 show as below.