Part Number: LMC567
Other Parts Discussed in Thread: LM567C
I AM TRYING TO MAKE A 2 TONE DECODER IN AN APPLICATION USING LMC567
It is low frequency: but signal is a 3.3v PULSE TRAIN out of a logic circuit.
The pulses at the input pin 3 of LMC567 have generally spectral content of 1200 Hz. I do not have an input coupling capacitor. Amplitude of either component would be in my estimates approx. 1.4v rms
But in some cases, the main spectral content of the input would be 400 Hz.
So I configured the VCO to be at 400 Hz so that output level is high most of the cases.
It should go low when the input pulses have very strong spectral content of 400 Hz.
But I do not see that. Output state does not change. I know from spectrum at the input that I do indeed have 120 Hz or 400 Hz.
I am suspecting that maybe the chip is not suitable for operation with pulse inputs which will have a broad range of frequencies.
Can I test the tone decoder operation by applying sinusoids by sweeping the signal over 400 Hz to 1220 Hz, say?
See pasted schematic in a ppt slide.ti_lmc567sch.pptx
The issue right now is: will the IC operate with these conditions of input signal and values?
thnx