This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Technical Support Team,
I'd like replace SN74LVC8T245 instead of TC74LVXC3245FS.
23pin of TC74LVXC3245FS is NC, but 23pin of SN74LVC8T245 is VCCB.
Is it possible to open 23pin of SN74LVC8T245?
Is SN74LVCC3245A more better to replace ?
Best Regards,
ttd
Hi Shreyas,
Thank you for your reply.
I'd confirm your comment.
>The NC pin can be left floating if the schematic and layout is done that way since there will be internal short between 1 &2 pins.
⇒23 & 24 of LVC8T245 pins are VCCB . Is it correct that both pins are internal short?
Best Regards,
ttd