Hi Team,
Linking another thread that I would have replied to in order to not add an additional thread, but it is locked and I am unable to do so. Isn't there supposed to be a new feature to make a new thread based off another one or something like that? https://e2e.ti.com/support/logic/f/151/t/589509?tisearch=e2e-sitesearch
Anyway, is down translation from 5V to 1.8V possible with this device when VCC is 1.8V? I know this will depend on the VIL, so the 5V signal would need to be a hard LOW and relaibly below ~0.55V MAX. Are there any other limiting factors?
A = 5.1V
B = 1.8V
VCC = 1.8V
Thanks!
Joe Stephan - FAE