I use LM567 as a PLL,get the output signal of pin 5.
The LM567 is locked with a square wave output from pin 5 of 500KHz,then to a AD8039 as the voltage follower,but the freq at the output of the voltage follower is moved to 539KHz,I was really confused about it.(I use AD8039 to remove the effect to the VCO freq in pin 5 by LC LPF),so the latter circuit goes wrong.
But when I give the AD8039 a 500KHz square signal directly from signal source,the output of the voltage follower is also 500khz,and the following circuit becomes normal.
So is my circuit of LM567 right?
I have try yet for using a dual chananel oscilloscope and connect the input of the ad8039/(pin 5 of LM567) to ch1 and the output to ch2,the freq becomes stable to 500KHz.If i move off the input pin,the freq at the output of AD8039 is shaking to about 539KHz again,Bying trying this for some times,the LM567 burned!
It's true that I should separate pin 5 and the lpf to get rid of freq pulling.