Part Number: LSF0108
Hi,
IBIS model having 1.2V, 1.8V, 2.5V 3.3V & 5V. But we need a level translator of 3.3V to 1.05V. But in IBIS model there is no 1.05V. And also Pins at A& B side (No:3to 18) having Terminator. But we need IO for those pins to perform Level translator operation. Could you please help us to resolve this issue. And please provide the IBIS model for LSF0108 which supports 1.05V also.
Regards
Anitha