This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC8T245: Multiple Direction Control

Part Number: SN74AXC8T245


I would to confirm that for the SN74AXC8T245 device, the B outputs are high impedance (tri-stated) when VCCB is powered with +3.3V while VCCA power is off, OE pin is tied to ground. 

  • Hi,

    As mentioned in the datasheet "The VCC isolation feature ensures that if either VCC input supply is below 100 mV, all level shifter outputs are disabled and placed into a high-impedance state." So by "power is off" you mean below 100mV then yes the outputs are placed into high impedance.

    Thanks!
    -Karan