The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] What is the maximum data rate (or operating frequency) for a logic gate or buffer?

Other Parts Discussed in Thread: SN74LVC1G34, SN74LVC1G79

FAQ: Logic and Voltage Translation > Timing Parameters >> Current FAQ

** NOTE **

This FAQ is in reference to push-pull output devices. Open-drain outputs will

inherently have slower operating frequencies due to the lack of a positive side driver.



Clock speed is not characterized for devices that do not include a clock input. This includes typical combinational logic gates (AND, OR, NAND, NOR, XOR, XNOR), line drivers (buffers, inverters, transceivers), and other combinational logic devices (encoders, decoders, logic multiplexers, etc.).

The maximum operating frequency can be estimated by finding a clocked device in the same logic family.

For example, the SN74LVC1G34 is a logic buffer, and does not include a maximum operating frequency.  The SN74LVC1G79 is a D-type Flip-Flop in the same logic family (LVCxG), and it includes an fmax value in the datasheet of 160 MHz (minimum).  This indicates that the SN74LVC1G34 can operate at 160 MHz also.