This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP2G17: Input Pull-Down Resistor

Part Number: SN74AUP2G17

Hello,

I am using the SN74AUP2G17 at the input of a digital circuit. I would like to know what is the required value of a pull down resistor so that the output doesn't float?

Thank you. 

  • Hi Ahmed,

    I'm not sure what you mean -- the output of the SN74AUP2G17 is a push-pull driver, which means it will never be floating.

    If you're talking about the input, then a 10kohm resistor will work fine in most circumstances.

    if you want to know how to properly size a pull-up resistor, we have an FAQ on that topic, located here:

    Please let me know if I can be of further assistance. 

  • "Pull-up and pull-down resistors are required in many logic systems to provide a valid logic state when a wire connected to a CMOS input is unused."

    Yes, this is my exact case because the buffer is located at the input. I asked because according to my knowledge, digital circuits in general can have an unexpected output if the input is not well defined (LOW or HIGH). For my application I assumed I need to pull down the input.

    The bottom line is that I want the input to be LOW when the input wire is not connected. Therefore the output would also be at a LOW state. On the other hand, when the input wire has a HIGH value, the output should be HIGH.
  • Hi Ahmed,
    So, the SN74AUP2G17 is connected to the CMOS input of another device - I understand that.

    You are correct that CMOS inputs need to be well defined (ie LOW or HIGH).

    My source of confusion comes from your use of the term 'input' without context -- the system you have described has 2 inputs and 1 output, one input and output on the SN74AUP2G17, and one input on the "digital circuit." (technically the 2G17 has 2 inputs and 2 outputs, I'm only considering 1 channel right now).

    I would recommend connecting a 10kohm resistor directly from the input that is to be disconnected to GND, regardless of which IC the input is on. This will allow the input to be controlled by a relatively weak driver, and it will hold the input at 0V when it is disconnected.
  • Yes exactly, I am using one of the SN74AUP2G17 inputs and the other is not used. I will connect a 10k resistor to the ground, and mark this question solved.

    Thank you.