This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E: overshot in TXS0104

Part Number: TXS0104E

Hi team,

My customer use the TXS0104 to transmit the voltage of SD card bus.

The schematic is as below:

The A port is 1.8V and B port is 3.3V.

And they see the over shoot in both A port and B port as below:

A port

B port

The voltage of the overshoot will not larger than absolutely value, but it is larger than the recommend value

  

So can you help to analyze the cause for the overshoot?

in addition, if the overshoot voltage is larger than the recommend VIH, what may be the cause for this? Does it cause the degradation in some specs?

Lacey

Thanks a lot!