This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC16T245: the relation between the Vih, Vil and Vi/o specs

Part Number: SN74LVC16T245


in the datasheep SCES636B,7.3 Recommended Operating Conditions,there is a table,Vih for data inputs is at line 3,Vil for data inputs is at line 4,Vi/o  is at line 8.according to the table, if Vcci=5V,Vcco=1.8V, then Vih min =3.5V,it is larger than Vi/o max at active state. that is the problem,because I want to use the SN74LVC16T245 in that case.Meanwhile,how much the data inputs voltage over Recommended operating Vcci and Vcco range is?