This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: TXB0108DQSR - RGB interface

Part Number: TXB0108

We are using TXB0108DQSR level translator for level translation of RGB interface from 3V3 to 1V8.

The Operating frequency is 20MHz.

Port A is connected to LCD and Port B is connected to Controller. VCCA=1.8V and VCCB=3.3V

The trace lengths of RGB signals in Port A of TXB0108 will be around 3 inches.

Will this work correctly?

 TXB0108DQSR RGB interface from 3V3 to 1V8.docx