Part Number: SN74AVC8T245
We used the AVC8T245_IO_33 model for SigXP simulation. The waveform shows non-monotonic falling edges which do not match the measurement. This is very obvious with the typical case. The slow and fast cases seem to be okay.
However, simulation with simple connection with no transmission line shows some shelf in the falling edge of fast, slow and typical cases. Removing the package effect, the falling edge became smoother. Add the package back in, the typical case shows up as a complete reversal. Fast and slow cases are not as noticeable.
See attached pdf for details.
Thank you.
Sheri