Part Number: LSF0108-Q1
Other Parts Discussed in Thread: SN74LVC1G07
Hi team,
If the low-side A power supply terminal is open, is the internal reference MOS gate fixed to the high-side B voltage?
The general connection is as follows.
I think that Vccb voltage appears at the Vref_A pin when Vref_A is open.
In that case, the switch gate voltage is Vccb, SW is always ON, and A1 and B1 are short-circuited.
If there is a internal pull-down resistor on the EN pin, this can be prevented.
Is there a internal pull-down resistor on the EN pin?
Best regards,
Tomoaki Yoshida