This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
If the low-side A power supply terminal is open, is the internal reference MOS gate fixed to the high-side B voltage?
The general connection is as follows.
I think that Vccb voltage appears at the Vref_A pin when Vref_A is open.
In that case, the switch gate voltage is Vccb, SW is always ON, and A1 and B1 are short-circuited.
If there is a internal pull-down resistor on the EN pin, this can be prevented.
Is there a internal pull-down resistor on the EN pin?
Best regards,
Tomoaki Yoshida
Hello Yoshida-san,
You are correct that if Vref_A is left open that the EN pin will be at 3.3V (in the above image). This will allow signals to pass from A1 to B1 or from B1 to A1, however the voltage will be clamped to ~2.5V (3.3V - 0.8V).
Clemens is correct - there is no internal pull-down resistor. You can setup an external circuit to disable the LSF device when the VrefA supply is disconnected:
* Screenshot from Using the Enable Pin with the LSF Family video.
An open-drain buffer such as SN74LVC1G07 can be used to force the EN pin to 0V if the VCCA pin is disconnected. Basically the input to the 1G07 would be coming directly from the Vref_A pin, and a pull-down resistor would have to be added at Vref_A (2.2kohm should work well).
Hi Emrys-san,
Thank you for your support.
I understand well.
I will consider countermeasure.
Best regards,
Tomaki Yoshida