Hello guys,
One of my customers has been used SN74LVC1G17 for many their products long time.
Their input signal voltage connected to the device "A" pin is -0.4V. So they always tested Vf of parasitic diode connected from "GND" pin to "A" input pin of all SN74LVC1G17 they use.
The Vf average volta was 0.7V~0.6V. But recently they found the Vf voltage was changed to about 0.46V. The Vf voltage went down from 0.6V~0.7 to 0.46V.
They want TI to answer the following questions. Could you give me your comments for them?
Q1. They know that Vf is changed by temperature and flowing current value.
They want to know whether the Vf is changed between factories of front end or not?
Q2. Also they want to know whether the Vf is changed between wafer material (ingot) lot?
Q3. What is Vf variation of parasitic diode connected from "GND" pin to "A" input pin roughly?
Your reply would be much appreciated.
Best regards,
Kazuya.