This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP2G00-Q1: How to design the gate's output?

Part Number: SN74AUP2G00-Q1

Hello,

I have some qeustions about NAND Gate(SN74AUP2G00-Q1).

1. There is Function table in the datasheet, but there is no information that two inputs are "X".

    What's the output level when two inputs logic is "X"?

2. If we want that NAND gate's output goes "L" when two inputs are "H", How we design the output default level? (Actually, we want that output level is "H" if any of two inputs are not "H".)

   Which is better pull-up or pull-down? Is floating best? If we sholud design using pull-up or pull-down resistor, could you recommend the value of resistor?

Thanks,

Manwoo Kim