Part Number: TXS0102
Hi,
The TXS0102's recommended low-level input voltage, VIL is 0.15V, which is too low even for AP from QUALCOMM, APQ8053, in which VOL max is 0.4V. But per notes in TXS0102, 'The maximum VIL value is provided to ensure a VOL is maintained. The VOL value is VIL plus the voltage drop across the pass-gate transistor'.
My questions are:
1. Does it mean even the actual VIL is higher than 0.15, for example, 0.4 of APQ8053, the VOL is simply 0.4+voltage drop? Because per block diagram of TXS0102, input and output are linked by a pass-gate transistor;
2. what is the value of 'voltage drop' across the pass-gate transistor? I need this value to evaluate the 'digital low' voltage of input and output voltage by using TXS0102.
Thank you very much and look forward to hearing from you soon.
Rgs/Sen.