This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G17: Used in Cascade connection and simulaiton models needed

Part Number: SN74AUP1G17


Hi Experts,

I have a request ot use SN74AUP1G17 for a cascade connection(above 20 stages) in the design, and wondering about the clock qualities would be after several stages. we plan to do the simulation to check this. Could you tell if I can get the simulation models(spice,or alternatives) to do this? If not, could you help check if it's feasible to do so?

basic setup like this:

Oscillator 50MHz-->5pF loading and SN74AUP1G17 --> 5pF loading and SN74AUP1G17--> 5pF loading and SN74AUP1G17--->…...-->5pF loading and SN74AUP1G17 ---> 5pF loading

regards,

Zhipei