The datasheet has the following regulations as electrical characteristics.
・ ∆t / ∆v Input transition rise or fall rate :
-VCC = 3 V to 3.6 V: 100ns / V (MAX)
When the above time was measured (*) with the product mounted on our board, it was about 208 ns / V, which is in excess of the regulation.
(*) Waveform measurement by oscilloscope at IC receiving end (5pin).
・ ∆t / ∆v Input transition rise or fall rate :
-VCC = 3 V to 3.6 V: 100ns / V (MAX)
When the above time was measured (*) with the product mounted on our board, it was about 208 ns / V, which is in excess of the regulation.
(*) Waveform measurement by oscilloscope at IC receiving end (5pin).
Does the above measurement result actually affect operation such as malfunction of logic IC?
Also, can you tell us about the specified value if there is an allowable range value in our evaluation?