Other Parts Discussed in Thread: SN74AXC4T245
This is regarding adding pull up resistors for the input pins to ensure a known state is defined. This is to prevent excess current draw during the High impedance state.
Do you define the input pins for A/B as when set by the 1DIR /2DIR pins. i.e. if DIR is set high. direction is A to B, So A is the input pin, not B. I just want to clarify if I require pull ups on the output side as well?
The second question I have is the sizing of the pull up resistor required. We have a battery run device, so current consumption is critical. I was hoping to use at least 100k, but after reviewing the calculation regarding switching characteristics (3.9ns max for 1.8V), also depend up trace capacitance, etc. Using Ct as 5pF, I calculate max pull up resistor of 1.9k approximately.
I was told we do not require pull up resistors, but after evaluating the part on an eval board (and seeing similar issues on this thread) , I was able to verify similar results (excess current draw during high impedance mode, VCCA line is powered down as well). I found installing pull ups on the inputs/and output does seem to solve the issue. I am currently determining if we require pull ups on the outputs. I am using 100k pull ups for this evaluation.
Thanks,
Mark