Other Parts Discussed in Thread: SN74LVC8T245
Dear Sir/Miss,
I gonna adopt SN74AXC8T245 as RGMII level shift between 1.8V and 3.3V. The topology and routing length are as below.Please help to confirm whether it works or not?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir/Miss,
I gonna adopt SN74AXC8T245 as RGMII level shift between 1.8V and 3.3V. The topology and routing length are as below.Please help to confirm whether it works or not?
Hey Milo,
Best way to determine if it will work will be to use the EVM and test using similar loads you expect. I can't confirm whether or not it will work in your system. However, i do know others have used this device for RGMII.
Milo,
you can also refer to the following app note which talks about RGMII level translation using AXC8T245.
The speed and prop delay is determined by the output loading, we have tested the AXC family to support the RGMII std speed ( exceeds 125Mhz) at the rated 15pF loading. with higher loading, the speed would probably decrease a bit but i believe it will still support 125Mhz. The skew as tested is within 500ps ( RGMII stds) for 1.8 <>3.3V translation.
Pull-up resistors would not improve the falling edges, and would make the signal asymmetrical.
To drive a higher capacitive load, you would need more drive strength, i.e., the SN74LVC8T245 (if it is fast enough).
Hi Clemens,
Thanks for your assistance.I want to replace AXC8T245 with AVC8T245.Please help to confirm whether it works or not? Whether the driving strength of the two sides of the chip are the same?For the longer signal of the trace, which side of the chip(A or B?) is used to connect?
Thanks
Milo
Milo,
as Clemens suggested, it seems that the drive strength of the AXC/ AVC is not sufficient for the signals to overcome the loading through the connectors and cables. You can switch to the LVC device which provides double the drive strength that is provided by the AVC/AXC devices for the same 3.3V level. ( 24mA)