This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G74: output when the power supply goes below 1.5 V

Part Number: SN74LVC1G74

Hi Expert,

https://e2e.ti.com/support/logic/f/151/p/877100/3245022

 

Regarding discussion about the output when the power supply goes below 1.5 V in the above session,

"The Recommended Operating Conditions table shows that the output value might change when the power supply goes below 1.5 V.

To ensure a known output state after power was interrupted, the processor must pull CLR low in that situation. (If the processor outputs go high impedance, you could add a pull-down resistor.)"


Question

Is it meaning, If customer pull CLR low, the output is fixed low even if Vcc<1.5V?

 

Thanks

Muk