This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G175: Detail Spec for the rising edge

Part Number: SN74LVC1G175
Other Parts Discussed in Thread: TLV7031

Hi, 

My customer want to know the detail spec for the rising edge for the SN74LVC1G175. We can't find the spec in the datasheet. Could you give some suggestions for this?

1. How about the detail spec for IC to judge the rising edage for the CLK pin? The threshold V? The rising time(the min value and the max value)?

2. Customer want to detect the rising edge for their system application. In a 5V supply system, they want to use a pulse as 100ms slow rising time with 3.2V high level at the CLK pin, can it make the Q flip to the high level? 

3. If not, do you have any suggestion to detect the rising edge for the CLK pin?