This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G17: Will level shifting 1.8V 50Mhz clock to 3.3V stable?

Part Number: SN74LVC1G17
Other Parts Discussed in Thread: SN74AUP1T17, SN74LV1T34, SN74AXC1T45

Hello,

I'm searching for a simple accurate clock level shifter to 3.3V for my 1.8V 50Mhz clock signals.

I came across the SN74LVC1G17, which was simple, cheap, small and had schmitt trigger feature for stable output.

However, the Vin threshold for Vcc 3V is MAX 1.92V, which should increase if the Vcc is 3.3V.

Does this mean I can't use SN74LVC1G17 to perform 1.8V to 3.3V level translation?

Could someone check if I'm misunderstanding the datasheet?

Thank You