This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCT04A: SN74HCT04A

Part Number: SN74HCT04A


Hi all,

As per the datasheet of SN74HCT04A, the Max. Value of VIL = 0.8 V which means the output should not go high till the input voltage goes below 0.8 V. 

But when I am simulating using the spice model in TINA - TI, my output is going from high to low when my input is going above 2.5 V and the output is going from low to high when the input is going below 2.5 V.