This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC74A: CLK input transition time

Part Number: SN74LVC74A
Other Parts Discussed in Thread: SN74HCS74

Hi Logic Experts,

My customer is using the SN74LVC74A in two different applications on the same design. I have a few questions. 

1. The datasheet specs the MAX transition rise/fall rate at 10ns/V. What happens if you exceed this rise/fall rate for the CLK input? My customer has a 5ns rise time for their 3.3V CLK input (1.5ns/V rate).

2. Does the device care if the rise and fall edges are very different timing? The CLK falling edge is 5ns in one use case but the rise edge is very slow at ~70us. 

Thanks!!
Reed