This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1T157: Rise Fall Rate Specification

Part Number: SN74AUP1T157


Regarding the [Input transition rise or fall rate] on the Datasheet, is the measurement point 10% to 90% and 90% to 10% respectively?

And about all of the TI's logic devices,  if there is no mention about the measurement point for the [Input transition rise or fall rate], is it 10% to 90% and 90% to 10%?

Thank you.